Vacuum Lifting Devices VacuMaster Window 200/300
- VacuMaster Window for vertical handling of windows, glass sheets and glass components
- Workpieces can be rotated to the side by 90°, with optional electric drive
- For lift capacities up to 300 kg
To provide the windows for shipping, the appropriate glass plates have to be taken from the standing bearing blocks and paned into the compatible window frame. Afterwards the windows are commissioned for transportation on mobile bearing blocks. This working process required hard, physical work, which was done by several employees. With a vacuum lifting device of Schmalz, the employees should be relieved and the production process accelerated.
The vacuum lifting device VacuMaster Window is the ideal solution for the handling of glass and windows. The vacuum lifting device VacuMaster Window is designed for loads with a weight up to 170 kg. Therefore with the lifting device the heavy glass plates can be handled easily. Due to the usage of two suction cups SPU, damaging of the surface is avoided. The lifting device VacuMaster Window convinces by its simple operability and ergonomic working by considering latest ergonomic knowledge. The glass plates can be turned to the left and to the right by 90 degrees. To take the glass plates undamaged from the glass bearing, the vacuum lifting device is combined with a bridge crane system ETK from Schmalz. The smooth aluminum crane construction in combination with the lifting device enable simple, safe and accurate commissioning of the plates and windows by only one employee.
Discover application examples of the product in various industries - user-friendly, informative and practical.
No suitable videos found? Then take a look at our media center.