Schmalz

Automated handling • Wood • Doors • Area Gripping Systems FXP

Vacuum Area Gripping System FXC for Flexible Handling of Doors With Various Dimensions

In the process of manufacturing doors, the workpieces are loaded into a CNC machining center. The doors have different dimensions and can include gaps, such as spaces for windows. The vacuum area gripping system FXC securely grips the various workpieces with ease.

The gripper system can handle different workpieces without requiring changes to the gripper. Even doors with a frame width of only 80 mm are no problem for the gripper system. The foam grid serves as the sealing element between the gripper and the workpiece. This sealing foam compensates for gaps in the workpiece which could cause leaks. The integrated valves open and close individual vacuum points according to how the gripper is covered.

The integrated vacuum generation creates a strong holding force with low energy consumption. The large-area gripping system with integrated vacuum generation reduces energy requirements by up to 50% compared to other conventional gripper systems on the market.

Show more
Product Inquiry

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart