Schmalz

Manual handling • Wood • Wooden sheets • Vacuum Tube Lifters JumboErgo

Vacuum Tube Lifter JumboErgo: For Loading and Unloading CNC Woodworking Centers

Previously, two employees were required to transport the coated wooden sheets to a CNC machine for processing. The employees were under extreme physical strain and their health was at risk as a result. To improve the process and relieve workers of this strain, the company purchased a vacuum lifting device from Schmalz.

The vacuum tube lifter JumboErgo can handle loads of up to 110 kg in weight without difficulty. The tube lifter is equipped with double suction cups. Since the two suction cups are fully adjustable on the crossbeam, they can even handle large, unwieldy sheets effortlessly. The wooden sheets can be lifted and lowered using the twist grip on the operator handle. A column-mounted slewing crane SK in combination with the vacuum tube lifter JumboErgo offers a complete solution. The column-mounted slewing crane SK enables access to the entire working area. In this way, the work can be completed by one employee ergonomically and with little physical effort.

Show more
Product Inquiry

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart