Schmalz

Holds its breath when the chips fly

Schmalz has developed a new vacuum block for metal and plastic cutting in CNC machining centers. The CMB-HD securely holds thin-walled workpieces and enables multiple machining steps in a single clamping operation. The ready-to-connect solution is also ideal when different clamping systems are used alternately.

The new CMB-HD vacuum block reliably holds thin-walled metal workpieces during the milling process.

Clamping flat and thin workpieces made of soft materials such as aluminum, plastic or brass without distortion is possible with vacuum. How? J. Schmalz GmbH demonstrates this with its new CMB-HD vacuum block. It is designed for use in CNC machining centers and holds even sensitive components securely thanks to its flat suction plate and high clamping force. It thus clears the way for the spindle to machine from five sides. The CMB-HD is the first vacuum block from Schmalz that users can easily attach directly to the T-slot table using clamping claws or to the zero-point clamping system using clamping bolts. The vacuum blocks can be used in both dry and wet machining processes.

Handy and well thought out

In addition to the vacuum, the calibrated frictional lining is responsible for the secure grip. It consists of the thermoplastic polyurethane TPU-70, which is both grippy and hard-wearing. As a result, it reliably absorbs even high lateral forces and ensures precise results. The specialist mounts workpiece stops for fast rough positioning of the parts to be machined as well as the vacuum feed directly on the aluminum main body. A pressure gauge monitors the vacuum close to the workpiece, thus ensuring safe operation. Magnetic holders are another safety-relevant accessory: They fix the vacuum connection set and the air hose to the machine table and prevent a collision with the tool during machining.

The new vacuum block makes it easier for companies with machining operations to get started with vacuum clamping. Since it can be set up quickly, it can be used flexibly - even when frequently alternating with other clamping devices. The CMB-HD is available immediately.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.