Schmalz

Search results

Filter results

Category

1 - 3 from 3 results

Press release

FQE-V gripper system: independent of size and shape

With the new FQE-V vacuum area gripper, vacuum expert Schmalz offers a freely scalable gripper system for robotics and automated handling of workpiece geometries of different sizes.With the new FQE-V, Schmalz has developed a modular, freely scalable gripper system for robotics. It enables workpieces of different sizes and shapes to be handled safely. Applications benefit from particularly fast project planning.Vacuum expert Schmalz has further developed the FQE series and supplemented it with the FQE-V. With dimensions ranging from 230 × 120 millimetres to 400 × 280 millimetres, the new area gripper is even more flexible in its dimensions and geometry. It therefore enables precise and safe handling of individually shaped workpieces, regardless of their format. The suction-plate dimensions and suction hole grid can be freely scaled. Applications can adapt the FQE-V to different workpieces quickly and easily using smart design tools. Batch size 1 thus becomes the standard.Schmalz offers this new development in two versions. The FQE-V-M is equipped with an external, the FQE-V-X with an integrated, particularly energy-efficient vacuum generator. This allows users to benefit from economical operation with a high level of process reliability. The control valves are also integrated. With its modular lightweight design, the new area gripper significantly reduces weight and thus increases the effective load capacity. Suction cups in different shapes and materials and foam are available as sealing elements. Sound insulation minimizes noise pollution for nearby employees.Users can choose from a wide pallet of suction trays with different shapes. These are rectangular, round or oval as standard. However, any free form can also be scaled - for example a T-shape. The innovative design of the FQE-V meets the requirements of ISO TS 15066 and is therefore ideal for stationary handling tasks in human-robot collaboration (HRC). The area gripper also impresses in automated handling - for end-of-line packaging in intra-logistics or for sensitive gripping of products in the automotive, glass and electronics sectors. The FQE-V enables the handling of objects from different pick-up positions. For example, it can dip precisely into workpiece layers in outer packaging or palletize non-rigid cardboard boxes. Because the gripper dimensions can be freely scaled, users can also use the FQE-V to fill goods in outer packaging layer by layer.

Video

Area Gripping System FQE-V Xc and Lightweight Layer Gripper ZLW for logistics applications

Flexible and precise handling of different products with Area Gripping System and Lightweight Layer Gripper. More information here!In this video, you will learn how our products, the Area Gripping Systems FQE-V Xc and the Lightweight Layer Grippers ZLW, efficiently and precisely handle small cartons. The Area Gripping System FQE-V Xc is a flexible gripper system designed for handling products of various sizes and geometries. It allows for picking up items from different positions and is commonly used in stationary applications with collaborative robots or in fully automated processes. Typical use cases include pick-and-place tasks, end-of-line packaging, and layer-wise filling of goods in outer packaging. With freely scalable gripper dimensions, the system can be precisely tailored to project-specific requirements. Its energy-efficient, integrated vacuum generation and low noise level make it both economical and workplace-friendly. The system is suitable for various industries, including packaging, automotive, glass, and electronics. The Lightweight Layer Gripper ZLW is specifically designed for automated palletizing processes and handling workpiece layers. With variable length and width, it adapts flexibly to different needs. Its lightweight design reduces initial costs by enabling the use of robots with lower payload capacities. The suction grid design is optimized for specific workpieces, further enhancing energy efficiency. The ZLW can handle a wide range of items, such as packages, pouches, jars, cans, and buckets. With optional features like a spring-mounted flange for height compensation and customizable sealing materials, it offers a versatile and adaptable solution. Discover in this video how these innovative systems can transform your operations!

Tradeshow

INNOVATION EXPO 2025 - International Logistics Exhibition

International Logistics Comprehensive Exhibition INNOVATION EXPO 2025Schmalz will exhibit at the Logis-Tech Tokyo INNOVATION EXPO 2025 to be held from September 10, 2025.Various products for the logistics industry will be exhibited, including manual transfer systems that support manual transfer of heavy loads and vacuum grippers that automate loading and unloading of pallets and other materials. Visitors can also try out a mobile tube lifter at the venue. We look forward to seeing you there.The International Logistics Exhibition (Logis-Tech Tokyo/INNOVATION EXPO) is Japan's largest specialized exhibition for the logistics and supply chain industry. In 2025, the event will be held under the theme “Keeping logistics moving. Driving society forward.” from September 10 (Wed) to 12 (Fri) at Tokyo Big Sight East Halls 4–8.Exhibit ProductsHighlightsTransportable tube lifter JumboFlex MobileThis is a transportable tube lifter that can be moved to any desired location. Its compact design not only allows it to be installed anywhere, but also makes it easy to maneuver during transportation. Driven by a 3-phase 200 V power supply, it can be used not only for temporary transshipment, but also for long processes such as feeding work into a processing machine.Customizable lightweight and vacuum gripper FQE-VRobot Demo: The FQE lightweight vacuum gripper is now available with a new type of suction surface that can be freely designed. The suction surface can be designed and manufactured with a 3D printer to match the size and shape of the workpiece. A robot demonstration will be held at the venue. Please come and see it.Rope balancer Neo30Rope balancer capable of lifting loads up to 30 kg. Battery-powered, it can be used anywhere, regardless of where it is installed. You can actually try it out at the venue.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart