Schmalz

Selection Aid for Vacuum Generators

Selection by Suction Rate

The necessary vacuum can be generated with vacuum generators of various types.

The following three vacuum generators are available:

1) Ejector
2) Vacuum pump
3) Vacuum blower

Each type has its own specific advantages, but they have one thing in common: a high suction rate at a high vacuum always means high power consumption and high operating costs.

Selection Aid for Compact Ejectors

Our selection aid for compact ejectors helps you find the right compact ejector for your application based on various technical properties.

Selection by Properties

This overview is available in PDF format in the following:

Checklist for Selection of Vacuum Generators

How is the vacuum generator driven?

Electrically (pump, blower) or pneumatically (ejector).

Is the workpiece air-tight or porous?

Affects the evacuation volume.

How large is the volume to be evacuated?

Details (in m³/h or l/min) are shown for each vacuum generator.

How long is the required cycle time?

Affected by: the evacuation volume of the vacuum generator, the volume to be evacuated, the switching times of the valves etc.

Which vacuum value is required?

For practical use, a value of -600 mbar is assumed for calculations with air-tight workpieces.

Where is the vacuum generator located?

Affects the size, weight and additional functions.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.