Schmalz

Vacuum Blowers

The blades (A) transport, accelerate and compress the air on the momentum principle. The air is dragged by the blades in this case. A vacuum is created at the suction end (B) this way. The compressed air (exhaust air) escapes through the outlet opening (C).

Blowers provide a very high suction rate due to the large air channel volume and specially shaped blades.

Advantages of vacuum blowers

  • Enormous suction rate
  • High leakage compensation
  • Evacuation of large volumes in a short time

Typical areas of application

  • Handling of porous workpieces, such as cardboard,
    insulation material, chipboards or bags

 

We distinguish between two basic types of vacuum blowers:

Vacuum blowers

  • Vacuum blowers are either directly driven or frequency-regulated.
  • Used especially for handling porous workpieces (chipboards, bags, etc.).
  • Frequency-controlled blowers can be customized by controlling the motor speed and respectively the suction rate.

Vacuum blowers with reversing

  • Vacuum blower with electro-pneumatic reversing for control of suction, blowing and neutral position.
  • Used for handling air-tight workpieces that are picked up and deposited quickly.

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen