- HIỆU QUẢ
Vacuum Blowers SB
- Suction rate from 75 m³/h to 1,250 m³/h
- Max. vacuum: 40 %
Hiển thị danh mục
The blades (A) transport, accelerate and compress the air on the momentum principle. The air is dragged by the blades in this case. A vacuum is created at the suction end (B) this way. The compressed air (exhaust air) escapes through the outlet opening (C).
Blowers provide a very high suction rate due to the large air channel volume and specially shaped blades.
Advantages of vacuum blowers
Typical areas of application
We distinguish between two basic types of vacuum blowers: