Schmalz

Vacuum Pumps

Vacuum pumps include an eccentrically mounted impeller with lamellas (A) which are pressed against the walls of the housing by centrifugal force and thus provide a seal. As the impeller rotates, the size of each chamber (B) varies. As the chamber becomes larger, the air in it expands and the pressure drops, resulting in a partial vacuum. The air is drawn in through the inlet (C), compressed and ejected through the outlet (D).

Due to their high compression factor, pumps generate a very high vacuum and according to the type, have a very high suction capacity.

Advantages of vacuum pumps

  • High vacuum with high evacuation volume

  • Central vacuum generation

Typical areas of application

  • As central vacuum generation in gantry handling systems

  • In manual vacuum handling systems

  • In packaging machines

We distinguish between three basic types of vacuum pumps:

Dry-running pumps

  • Universal vacuum pumps requiring little maintenance

  • Used mainly as central vacuum generator in large gripping systems for handling air-tight workpieces

Oil-lubricated pumps

  • Vacuum pump with extremely high vacuum level (up to 95% vacuum)

  • Used in handling systems with an emphasis on low noise and low maintenanceas well as high vacuum, for handling air-tight workpieces

Water-ring pumps

  • Vacuum pump requiring little maintenance with internal water cooling for handling air-tight workpieces

  • Used especially in areas with high demands on ambient air (e.g. packaging in the food industry

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.