Schmalz

Vacuum Pumps

Vacuum pumps include an eccentrically mounted impeller with lamellas (A) which are pressed against the walls of the housing by centrifugal force and thus provide a seal. As the impeller rotates, the size of each chamber (B) varies. As the chamber becomes larger, the air in it expands and the pressure drops, resulting in a partial vacuum. The air is drawn in through the inlet (C), compressed and ejected through the outlet (D).

Due to their high compression factor, pumps generate a very high vacuum and according to the type, have a very high suction capacity.

Advantages of vacuum pumps

  • High vacuum with high evacuation volume

  • Central vacuum generation

Typical areas of application

  • As central vacuum generation in gantry handling systems

  • In manual vacuum handling systems

  • In packaging machines

We distinguish between three basic types of vacuum pumps:

Dry-running pumps

  • Universal vacuum pumps requiring little maintenance

  • Used mainly as central vacuum generator in large gripping systems for handling air-tight workpieces

Oil-lubricated pumps

  • Vacuum pump with extremely high vacuum level (up to 95% vacuum)

  • Used in handling systems with an emphasis on low noise and low maintenanceas well as high vacuum, for handling air-tight workpieces

Water-ring pumps

  • Vacuum pump requiring little maintenance with internal water cooling for handling air-tight workpieces

  • Used especially in areas with high demands on ambient air (e.g. packaging in the food industry

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

URL-osoite, jota yrität käyttää, ei ole oikeassa kieli- tai maakontekstissa.

Tiliin liittyvä myymälän kanava ei vastaa pyydetyn URL-osoitteen kanavaa. Jos haluat tarkastella hintoja tai tehdä tilauksen, vaihda käyttäjäkohtaiseen kanavaan.

0 tuotteet lisätty onnistuneesti ostoskoriin

Mene ostoskoriin

Schmalz Select - Suositeltava tuotevalikoima alipainetegnologiaan

Kaikki saatavilla. Kaikki valmiina. Kaikki selvää.

Select-valikoiman avulla voit luottaa hyväksi todettuihin vakiotuotteisiin, jotka ovat välittömästi ja maailmanlaajuisesti saatavilla ja joita voidaan yhdistellä optimaalisesti. Ei enää pitkiä toimitusaikoja ja epävarmuutta tuotteiden valinnassa. Löydät juuri tarvitsemasi komponentit - nopeasti, mutkattomasti ja maailmanlaajuisesti saatavilla.