Schmalz

Even more flexible: Schmalz expands the range of applications of the VCBL-GL vacuum block

Vacuum specialist Schmalz has further developed the VCBL-GL vacuum block. The new generation impresses with a modular design, an extensive spare parts catalog and a wider range of applications - for more flexibility and lower costs over the entire life cycle.

The VCBL-GL vacuum block is ideal for clamping glass.

The tried and tested VCBL-GL delivers what it promises. Schmalz originally developed the vacuum block for the special grinding and cutting of glass workpieces on smooth table machines from the Japanese manufacturer Bando Kiko. The vacuum specialist stocks all standard heights used in the glass industry as standard. And thanks to the modular design, special heights can also be implemented on inquiry. This innovative solution is now also suitable for other industries, such as stone processing. Among other things, this is made possible by the new triple sealing, which holds the vacuum even more reliably and offers more - especially for demanding applications. With its high transverse pick-up, the suction cup fixes them safely and gently - and they can be dry or wet.

Schmalz has designed the new version to be even more modular for maximum flexibility: Individual assemblies can be easily replaced, combined or adapted - which also makes servicing and maintenance easier. Thanks to an extensive spare parts catalog, applications benefit from higher availability and lower overall operating costs. The modular design also makes it possible to reduce the purchase price by up to 40 percent compared to the previous version.

The VCBL-GL-C for glass processing is available in various basic geometries - square, rectangular or in special shapes such as triangular. Individual inquiries can also be addressed with flexible heights. Schmalz manufactures the upper suction plate individually according to customer data, while the base plate is optimally matched to the clamping surface. This means that every workpiece can be clamped efficiently and accurately.

The VCBL-GL-C offers a special highlight with its reversing function: applications can handle mirrored components with just one suction cup. The special friction material enables high lateral force absorption and precise machining even with high forces. With a height tolerance of ±0.05 millimetres, replaceable sealing cord and robust aluminum base body, the VCBL-GL is precise, economical and robust. This makes it suitable for continuous operation in series production.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico

Schmalz Select – Preferred Product Range for Vacuum Technology

All available. All set. All clear.

With the Select portfolio, you can rely on proven standard products that are immediately and globally available and can be optimally combined. No more long delivery times and uncertainty when choosing products. Find exactly the components you need – fast, uncomplicated and available worldwide.