Schmalz

Down to the purest detail – purity without compromise

In sensitive production environments, cleanliness and hygiene are not an option, but a matter of survival. Even the smallest mistake – whether due to contamination, unclean handling or inefficient processes – can have enormous consequences: Loss of quality, damage to consumer health, loss of production, damage to image or even legal consequences.

In order to meet these high requirements, different concepts are used, each pursuing specific protection goals. This is precisely where two worlds meet, which at first glance appear to be different and yet pursue a common goal: cleanrooms and hygienic areas. While cleanrooms are primarily focused on particle and germ freedom, hygienic areas concentrate on protection against microbiological contamination and infections. Different approaches – one common claim: uncompromising protection against contamination and process safety.

Purity & hygiene fact check

80%

of contamination in a cleanroom is caused by people, especially by skin flakes or clothing.

0,1

micrometers is the particle size that is filtered out by cleanrooms. By comparison, a human hair has a diameter of around 70 micrometers.

1.000.000

particles per minute can be released from textiles. This is why special cleanroom clothing is essential.

85%

of infections can be prevented in hygienic areas through consistent cleaning and disinfection.

Purity in cleanrooms and hygienic areas is more than a standard to us. It is our commitment to quality and process reliability.
∼ Matthias Müller, Head of Sales, Vacuum Automation

Handling in sensitive areas

Handling in hygienic areas and cleanrooms requires strict measures to prevent contamination and comply with cleanliness standards. This includes the use of suitable personal protective equipment (PPE) such as protective suits, gloves as well as mouth and nose protection, regular hygiene training and the correct use of auxiliary and operating equipment such as lifting devices.
Quick movements and frequent surface contact must be kept to a minimum, and tools and materials must be sterile and disinfected. Cleaning, decontamination and maintenance processes, including the maintenance of ventilation systems, ensure that cleanliness is permanently safe. These measures ensure product quality and process reliability.

Vacuum technology combines both worlds

This is precisely where Schmalz comes in with its specially developed vacuum automation and handling solutions for handling in cleanrooms and hygienic areas. Our products and systems are an integral part of modern cleanroom technology and make a decisive contribution to avoiding contamination and reliably complying with cleanliness standards.

Two worlds, one claim: absolute purity

Two worlds, one claim: absolute purity

MORE ABOUT CLEANROOMS

MORE ABOUT CLEANROOMS

MORE ABOUT HYGIENIC AREAS

MORE ABOUT HYGIENIC AREAS

Contact

If you have any questions, we will be happy to assist you.
Schmalz d.o.o.

Velika Ligojna 4
Vrhnika

Slovenija
+386 70 613 796
info@schmalz.si
Contact
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico

Schmalz Select – Preferred Product Range for Vacuum Technology

All available. All set. All clear.

With the Select portfolio, you can rely on proven standard products that are immediately and globally available and can be optimally combined. No more long delivery times and uncertainty when choosing products. Find exactly the components you need – fast, uncomplicated and available worldwide.