Schmalz

Manual handling • Wood • Furniture parts • Vacuum Tube Lifters JumboErgo

Vacuum Tube Lifter JumboErgo for Loading and Unloading of a CNC Woodworking Center

To transport the heavy wooden sheets and to load the CNC woodworking center, two or more employees were necessary before. These had to do hard, physical work. To reduce costs and and enable ergonomic, health protecting working, the company decided to buy a vacuum tube lifter from Schmalz.

The vacuum tube lifter JumboErgo enables the handling of heavy wooden sheets and is designed for loads up to 120 kg. The wooden sheets can be lifted and lowered fast, precisely and flexible due to the twist grip directly on the operator handle. Thanks to the pneumatic swivelling unit PSE smooth swivelling by 90 degrees is enabled.The vacuum tube lifter JumboErgo is equipped with a double suction gripper. The two suction cups are steplessly movable on the main beam. Combined with a column-mounted slewing crane SK from Schmalz the JumboErgo is the perfect handling solution.

Show more
Product Inquiry
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico