Ejector Modules
- Small and compact vacuum generators
- For centralized and decentralized vacuum generation
- Integrated silencer
Pneumatic vacuum generators function based on the Venturi principle
Compressed air is introduced into the ejector (A)
Due to the reduced cross-section of the motive nozzle (the Venturi nozzle [B]), the compressed air is accelerated. The dynamic pressure increases, while the static air pressure simultaneously decreases.
Once it has passed the motive nozzle, the accelerated air expands and a vacuum is generated
Air is "sucked" through the vacuum connection (D) into the ejector
The compressed air escapes from the ejector through the silencer (C) together with the "sucked-in" air.
Vacuum generators that function according to the Venturi principle are especially suitable for very high accelerations
Vacuum grippers can be controlled individually
Ejectors in different designs for centralized and decentralized vacuum generation depending on the application
Various power classes to suit the workpiece and application
Pneumatic operation with integrated vacuum generation
Compressed air escapes through holes in the suction cup and is greatly accelerated when doing so
Due to the increase in speed, the static pressure falls and a vacuum is produced (A) ("Bernoulli Equation")
The accelerated air escapes to the side (B); an "air cushion" is produced between the floating suction pad and workpiece
Leakage is compensated for through a high flow rate, which means that even porous workpieces can be handled and separated
The Bernoulli effect ensures that the workpieces are handled with minimal contact
Floating suction cups function according to Bernoulli's principle
Low-contact, gentle handling of thin and sensitive workpieces thanks to the Bernoulli effect
Safe separation of thin and porous workpieces
Pneumatic operation with integrated vacuum generation
With the Coanda principle, compressed air is guided through an annular gap which accelerates it
The increase in the flow speed results in the "Coanda effect" in which the escaping air follows a convex surface
The air flowing along the surface produces suction ("entrainment") in the ambient air
High suction rate and low air consumption (the required operating pressure is 1 to 5 bar) due to the Coanda effect
Large contact surface with narrowly positioned vacuum openings prevent the workpiece from being sucked in or damaged
Suction areas can also be partly engaged