Schmalz

Manual handling • Metal / Sheet metal • Metal sheets • Vacuum Lifting Devices VacuMaster Eco

Vacuum Lifting Device VacuMaster Eco Provides an Energy-Independent Solution for Handling Aluminum and Metal Plates

To process aluminum plates weighing up to 250 kg on a CNC machine tool, loading used to be done by hand. This task required at least two employees. To relieve the strain on these employees and protect their health, the company decided to make a change.

The vacuum lifting device VacuMaster Eco provided the perfect solution for horizontally lifting the aluminum and metal plates and depositing them for the CNC machine tool. The advantages of the VacuMaster Eco lifting device include that it does not require an external energy source. This means that this lifting aid is especially flexible in use. The battery-operated warning device with battery test function ensures a high degree of work safety. In this case, the vacuum lifting device was designed for a maximum load of 250 kg and can be operated by one person. The company is thrilled about the resulting 50% reduction in personnel costs and highly satisfied.

Show more
Product Inquiry

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.

0 products successfully added to cart

Go to shopping cart