A barrel of colors - ergonomics meets colorfulness
With the VacuMaster, even heavy 200-liter barrels can be moved effortlessly.
A Great Place to Work 2023 and therefore one of the best employers in Baden-Württemberg: Emil Frei GmbH & Co. KG, brand name FreiLacke, was able to impress both its employees and the competition jury. "One of the reasons is certainly that we attach great importance to ergonomic workplaces," says Dr. Rainer Frei, Managing Director and Commercial Director. "Our staff are the guarantors of our great success and we support them. Of course, this includes reducing physical strain wherever possible." Specifically, for example, at the packing stations. Several hundred parcels weighing 25 kilograms each and heavy barrels have to be moved here every day. "That adds up to several tons per shift," emphasizes Oliver Zanner, Head of Marketing at FreiLacke. The solution: vacuum lifting devices from Schmalz. The operation also uses many of the lifting devices for handling raw materials and in the production areas.
In discussions with the sales department, it became clear that the VacuMaster solution planned individually for us would deliver the best result - and that's exactly what happened. It is only thanks to the lifting aid that we are able to handle the heavy barrels without putting any strain on our employees. That's great!∼ FreiLacke logistics manager Frank Januschowski
Founded in 1926, the family-owned company FreiLacke produces custom-made colors and coatings for customers in the vehicle, machine and apparatus construction, contract coating, functional furniture, storage technology, construction and sanitary sectors, as well as for rail vehicles and the wind energy industry. This includes liquid coatings as well as powder and electrophoretic coatings and composites solutions. In 2023, more than 650 employees generated annual sales of around 180 million euros at the Bräunlingen-Döggingen location in the southern Black Forest. The system coating specialist's products are sold to industrial customers worldwide.
Individually planned
FreiLacke has been benefiting from the excellent ergonomics of the vacuum lifters and crane systems from Schmalz since 2010. The solutions from Schmalz greatly reduce the load for personnel when lifting. This supports the back and musculoskeletal system. This is confirmed by the independent association Aktion Gesunder Rücken e. V. (AGR) with its seal of approval.
"Thanks to the VacuMaster, we can also pick our industrial coatings ergonomically in 200-liter barrels," emphasizes Oliver Zanner.The VM-Basic-270-1 vacuum lifting device enables effortless and health-friendly handling of even very heavy workpieces. Without this lifting device, barrels weighing at least 250 kilograms would not have been an option as transport containers."We use a completely customized solution that Schmalz designed for us." The modular design made this possible. FreiLacke received the lifting aid that was exactly right for the application thanks to the selection of different basic modules, operator handles, load beams and suction plates.
The vacuum generator is located in the basic module and provides the necessary suction force to the lifting device, which transfers it to the workpiece via the suction plates. The aluminum load beam also serves as a vacuum reservoir. The system works on an overhead crane, which allows for a large reach, and a chain hoist takes over the lifting force. This allows the skilled workers to effortlessly place the heavy barrels, which come from the storage area by forklift, on the Euro plates ready for dispatch.
Almost like riding a motorcycle
FreiLacke uses several JumboErgo-65s for handling smaller shrink wrapped goods. These vacuum tube lifters move the 25-kilogram shipping cartons for powder coatings just as sensitively and precisely as the buckets - filled with twelve kilograms of liquid coatings and without straining the skilled workers. "This has allowed us to minimize work-related musculoskeletal disorders among our pickers," says Oliver Zanner happily. A colleague from the shipping department, who works with the Schmalz devices on a daily basis, adds that one detail is convincing: "Before we used the Schmalz solution, we had a few mishaps because the adhesive tape on the cardboard boxes failed or buckets were not closed properly," he recalls. "The suction cups keep boxes and cans safe during movement and place them exactly where they are needed." Using the twist grip, employees lift, lower and release the load without effort. "It's as easy to operate as accelerating a motorcycle, and it's fun," he says.
Depending on the handling task, the specialists use the appropriate end effector, which they can change in a few simple steps thanks to the quick-change adapter: The round vacuum gripper RG moves the paint buckets, and the double suction cup DG and the four head suction cup VG pick up large cardboard boxes safely. Both solutions are adjustable and can therefore be adapted to any workpiece. Large stacking heights are no problem thanks to the movable operator handle.
Maximum reach is also ensured here by jib cranes, on which the tube lifters are moved horizontally along the ceiling for several meters. Thanks to the large swivel angle of 180 degrees, the lifting aids can even reach areas that are difficult to access. The cranes are designed for loads up to 65 kilograms and are responsive thanks to their aluminum construction. Another advantage: thanks to the large swivel angle, only one JumboFlex is required for two packing stations.
Optimal solution for every task
FreiLacke also uses several JumboFlex-35 vacuum tube lifters, which the skilled workers can operate intuitively with one hand, allowing them to move workpieces weighing up to 35 kilograms over long periods of time without tiring. The suction cups on this model can also be exchanged using the quick-change system and adapted to different loads.
FreiLacke logistics manager Frank Januschowski appreciates the uncomplicated cooperation with Schmalz. He regularly visits trade shows such as LogiMAT with colleagues to find out about new products. Together with the vacuum experts, he considers how the ergonomics in the company can be further improved. "In discussions with the sales department, it became clear that a solution planned individually for us would deliver the best result with the VacuMaster - and that's exactly what happened. It is only thanks to the lifting aid that we are able to handle the heavy barrels without straining our employees. "That's great," he sums up, and another thing is convincing: "We've been using some of the lifting aids for many years. If our requirements change, Schmalz takes care of the conversion. This means we always work with the best possible equipment."
Schmalz designed the basic module, operator handle, load beams and suction plates of the VacuMaster individually for the application at FreiLacke.
Thanks to the movable operator handle on the JumboErgo-65, employees can reach great stacking heights.
The double suction cup DG on the JumboErgo holds the parcels safely.
Overhead cranes provide the necessary reach for the lifting aids.
The JumboErgo-65 can be used flexibly on the swivel-mounted overhead crane wherever it is needed.
Media contact
The Schmalz press team will be happy to answer any questions you may have.