Schmalz

Distributor Selection

The distributor has to match the used hose diameter and the number of suction cups.

Example:
The hose VSL 8/6 has an outside diameter of 8 mm and an internal diameter of 6 mm. Six suction cups are used.

For this example we choose:

Plug-in screw unions STV-GE G1/4-AG 8 for the hose VSL 8/6 with outside diameter 8 mm and internal diameter 6 mm as well as 1/4" thread matching the female thread of the distributor.

Plug-in screw union STV-GE G3/8-AG 8 fits the spring plunger.

Distributor VTR G3/8-IG 9xG1/4 with one input (3/8" thread) and nine outputs (1/4" thread).

Three sealing screws VRS-SB G1/4-AG to close the three open outputs.

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.
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
Select 포트폴리오를 사용하면 전 세계에서 즉시 사용 가능하고 최적으로 조합할 수 있는 검증된 표준 제품을 신뢰할 수 있습니다. 더 이상 긴 납품 시간과 제품 선택의 불확실성이 없습니다. 빠르고 복잡하지 않으며 전 세계에서 사용 가능한 필요한 진공 부품을 정확하게 찾아보세요.