Schmalz

Jib crane

Aluminum jib cranes from Schmalz are responsive and ergonomic. The crane rails and pivot bearings are made from aluminum, which means less effort is required to swivel the jib. 

Even heavy loads weighing up to 1000 kg can be lifted safely and with little physical effort. Jib cranes from Schmalz can be combined with many lifting devices such as chain hoists, cable hoists, cable balancers or vacuum lifters. Depending on the installation conditions, customers can choose between a column-mounted jib crane or a wall-mounted jib crane. Schmalz also offers special designs for rooms where space is limited: a flat jib for low ceiling heights, an articulated-arm jib to move around obstacles and telescopic jib for difficult-to-reach work areas.

Zoek uw contactpersoon

Jib cranes from Schmalz are highly flexible

Jib cranes from Schmalz can be equipped with aluminum or steel crane rails, depending on the maximum required load. With aluminum jib cranes, even heavy workpieces of up to 650 kg can be handled safely and in a health-friendly, health protective manner. They convince by perfect responsive and maximum ergonomics.

The crane is equipped with steel crane rails as soon as a load of more than 650 kg is to be lifted. The jib cranes can thus move workpieces weighing up to 1,200 kg. To further increase ergonomics, it is possible to equip the crane movements with electrical drives.

Crane systems from Schmalz can be combined with the SCH chain hoist, rope balancer or chain hoist with lifting device and are therefore very versatile. They are designed in the standard version for indoor use, but special solutions for outdoor use are also available on request. Likewise, Schmalz offers special jib cranes with articulated-arm jibs, telescopic jibs or particularly flat jibs, and a special design for hazardous areas make Schmalz cranes all-round talents you can rely on.

In combination with a vacuum tube lifter or a vacuum lifting device, jib cranes from Schmalz form complete systems that are ready to connect.

Jib cranes can be divided into two types: Column-mounted jib cranes and wall-mounted jib cranes.

Column-mounted jib crane

Column-mounted jib cranes consist of a jib arm mounted on a stable base. Column-mounted jib cranes from Schmalz can be mounted anywhere in the room and have a swivel angle of up to 270°. For example, the swivel angle can be limited as desired with the help of the extensive range of accessories. The base plate GP enables the jib crane to be moved quickly and easily using a lift truck or forklift. This means that column-mounted jib cranes from Schmalz are always right where they are needed.

Wall-mounted jib crane

Wall-mounted jib cranes can be mounted directly on an existing wall or column on site and therefore do not require their own base. Schmalz wall-mounted jib cranes have a swivel angle of up to 180°, which can be limited as desired with the optional slewing angle limiter SWBG. The special, newly developed wall brackets for mounting the jib crane make mounting quick and easy. With the help of the extensive accessories, the wall-mounted jib crane can also be adapted to the individual requirements of the application.

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.