Schmalz

Vacuum Lifter Plates

Vacuum lifters for sheets made of various materials including wood, sheet metal, glass and stone are devices in materials handling that are able to lift, move and deposit heavy sheets with the help of a vacuum. The range of Schmalz vacuum lifters is divided into two categories: the vacuum tube lifter Jumbo and the vacuum lifting device VacuMaster:

  • Vacuum Tube Lifter Jumbo

  • Vacuum Lifting Device VacuMaster

We will find the right solution for your sheet handling application: Selecting the right vacuum lifter for your application depends on the maximum weight of your workpieces as well as the type of handling and alignment. In the wood industry, vacuum lifters ensure efficient loading of CNC machining centers or panel dividing saws and meet the highest requirements when it comes to swiveling or turning workpieces, for example. When handling steel sheets or metal, CNC laser cutting machines are loaded and unloaded, and fragile windows and heavy glass sheets are effortlessly moved by one person in a way that is protected against breakage. Vacuum lifters also ensure efficient material flow in other sectors. Schmalz is a proven partner when it comes to supplying vacuum lifters and crane systems — from universal devices to customer-specific solutions.

Zoek uw contactpersoon

Options for Handling Materials Such as Wood, Sheet Metal, Glass Sheets or Stone

Choose between different vacuum lifters depending on the application:

  • Workpieces weighing up to 300 kg can be moved quickly and efficiently using the vacuum tube lifter Jumbo. This device is usually used for porous and air-permeable workpieces such as cardboard boxes, sacks or wooden boards.

  • With the vacuum lifting device VacuMaster, heavy loads weighing up to several tons can be handled ergonomically and safely. It is often used for smooth and airtight workpieces such as metal plates and glass sheets.

Vacuum Tube Lifter Jumbo

Products

Vacuum Lifting Device VacuMaster

Products

The Right Schmalz Crane System for Every Vacuum Lifter for Sheets

To ensure ergonomic handling of sheets with the vacuum lifter, Schmalz can help you choose the right crane system. The aluminum crane systems and jib cranes have been precisely adapted to the lift capacities of the vacuum lifters. The modular system allows the vacuum lifter and crane system to be easily integrated into your working environment.

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.