Schmalz

LQE compact valve from Schmalz: fast, smart, safe

The LQEc/i compact valve significantly shortens the suction and depositing time for workpieces: It is so small and light that it can be installed directly on the gripper and provides the vacuum as required in fractions of a second.

The LQE compact valve guarantees extremely fast evacuation and ventilation times.

Maximum throughput in pick-and-place applications requires a high-performance gripping concept. The prerequisite for this: extremely short evacuation and ventilation times. This is where the directly actuated 3/2-way valves LQEc/LQEi with integrated vacuum switch from Schmalz come into play. In systems with centralized vacuum generation, they enable decentralized monitoring and control of the process directly at the gripper. Thanks to the design as a bistable valve with end position fixing and the additional non-return valve, the vacuum is held and process reliability is ensured even in the event of a power failure.

With a maximum flow rate of 268 liters per minute, the compact valves can be used either individually or together for the design of multiple vacuum circuits. In combination with electrical vacuum generators such as the Compact Pump GCPi, operators can design fully electrical systems. The effective atmospheric ventilation makes it possible to completely dispense with expensive compressed air, even when depositing workpieces. Optimized flow cross-sections make the process fast and reliable. Connectors and the start of operations are completed quickly, as the valve and switch are integrated into the housing.

LQEi is part of the Schmalz Connect series and is therefore predestined for the digital factory. It provides process and status data at all times via IO-Link - so not only can specialists monitor the machine remotely and in real time, they can also detect creeping changes before a failure occurs.

Safe in the process: If the vacuum generator fails, the LQE seals and maintains the vacuum on the gripper.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico