Vacuum Tube Lifter JumboFlex is a Flexible Tool that Helps You to Move Cardboard Boxes Quickly
When the logistic department receive incoming cardboard boxes, every wooden pallet must be replaced by a plastic pallet. This is due to the pharmaceutical industry's hygiene regulations. Previously, it took two people to move cardboard boxes by hand, which weigh as much as 25 kg. The company wanted to make the work easier by installing a lifting aid. Their special requirements were the space constrictions and the limited room height in the incoming goods area.
The vacuum tube lifter JumboFlex is ideal for rooms with low ceilings. Loads are gripped and lifted using vacuum force alone. Thanks to the low weight of the lifting solution and a compact design, it can be used even in tight spaces. The cardboard boxes are moved efficiently by only one person, thus reducing personnel costs by 50%. With a monorail fixed to the ceiling, optimum use of the vacuum tube lifter is possible within the available working area.
Videa
Objevte příklady použití produktu v různých odvětvích - uživatelsky přívětivé, informativní a praktické.
Nebyla nalezena žádná vhodná videa? Pak se podívejte do našeho mediálního centra.