Schmalz

Vacuum Technology for the Electronics Industry

Clean and Flexible Handling

With increasing digitization and connectivity in almost every industry, not only the demand for electronic components is increasing, but also their complexity. In the automotive, consumer electronics (handsets), infrastructure and aviation sectors, for example, the demands placed on parts and components are constantly increasing. New production technologies and miniaturization are the results.

In the semiconductor sector, increasingly better and more powerful chips are manufactured, which are further processed in complex processes in the packaging sector. Due to the steadily decreasing form factor, PCB manufacturers and developers are required to generate more complex circuits and to manufacture them reliably. The high demand for electronic devices also requires manufacturers in all areas to improve their processes, increase throughput and achieve YIELD increases. Automation and information processing are part of this process. Safe and sensitive handling of components and products within the process chain are becoming increasingly important.

Vacuum technology and the associated vacuum systems make it possible to meet the requirements. Thanks to Schmalz's expertise in the field of vacuum technology and the associated knowledge of the electronics industry, Schmalz can offer the right solutions for the most advanced processes. In addition, new products are constantly being developed to meet the increasing requirements in the individual areas of semiconductor, printed circuit board and end product production.

Tuotekysely

Uusi

Webinaari: Oikea imukupin materiaali herkille elektroniikkakomponenteille

Haasteesta käytännön ratkaisuun:

Tässä nauhoitetussa webinaarissa opit, miksi tavalliset imukuppit tulevat nopeasti äärirajoilleen käsiteltäessä herkkiä elektroniikkakomponentteja - ja ennen kaikkea, miten nämä haasteet voidaan voittaa.

Käytännönläheisen tarkistuslistamme avulla oikeiden materiaalien ja imukuppien valintaan saat konkreettista opastusta omaan sovellukseesi.

KATSO WEBINAARI NYT - 100 % ILMAINEN JA TÄYSIN JOUSTAVA

  • Saatavilla ilman aikarajoja - katso milloin sinulle sopii

  • Siirry suoraan sinulle tärkeimpiin osioihin

  • Kaikki sisältö pysyvästi saatavilla

Katso webinaari nyt!

Schmalz offers you the suitable solution in the electronic industry

Click on the individual areas to learn more.

1
Vacuum Technology during the Manufacturing of Printed Circuit Boards
2
Vacuum Technology for Printed Circuit Board Assembly
Vacuum Technology during the Manufacturing of Printed Circuit Boards

Requirements for Vacuum Technology

The active areas of the printed circuit board are highly sensitive, therefore the PCBs are handled at the outermost edge. As a result, Schmalz recommends the use of suction cups with a diameter of less than 15 millimeters from the PFYN, FSGA or FSG product families. The use of a spring plunger for height compensation from the FSTIm product family supports safe handling. In combination with a flat suction cup like the SGON, this results in a solution that masters even the most difficult requirements and load cases.

In the field of PCB manufacturing, environmental influences should not be underestimated. Schmalz offers a wide variety of materials in combination. The product portfolio includes suction cups made of low-impression HT1 material as well as NBR-ESD material for the safe discharge of generated charges.

Thanks to the individually adaptable solutions from Schmalz, handling and process steps can be made safer and rejects minimized.

Product recommendations for Use in the Manufacturing of Printed Circuit Boards

Vacuum Technology for Printed Circuit Board Assembly

Requirements for Vacuum Technology

Due to the diversity and countless geometries of an assembled printed-circuit board, a PCB handling solution is required that compensates for the height differences of the components while also preventing damage due to mechanical stress. Thanks to its extremely high flow rate, the Schmalz flow gripper SCG is ideal for handling circuit boards and uneven components. The sealing lip adapts to the different geometries. The partially projecting solder tags used in the THT process create height differences that can be compensated by the floating suction cup SBS (based on the Bernoulli principle), thus enabling effective handling.

Vacuum technology is used not only in the assembly process itself, but also for the component supply station ("feeder") of the pick-and-place machines. Whether for the blister tape reels ("Tape&Reel") or the tray supply: Schmalz suction cups can be used to great effect in both areas. Schmalz also offers suitable products for larger components and for provision in plastic tubes.

Product recommendations for Use in Printed-Circuit Board Assembly

Asiakirjat
Asiakirjat
Kieli

Sähköstaattinen purkaus: Sähköpurkauskapasiteettia koskevat vaatimukset

Elektroniikkateollisuudessa työkappaleet altistuvat usein äärimmäisille rasituksille erityisesti valmistus- ja käsittelyprosessien aikana. Mekaaninen tai terminen rasitus ei ole ainoa syy komponenttien tai materiaalien vaurioitumiseen.

Sähköstaattiset varaukset ja niistä johtuva hallitsematon sähköstaattinen purkaus (ESD) aiheuttavat peruuttamattomia vaurioita sähköisille, elektronisille tai optoelektronisille komponenteille, kuten IC-siruille tai piirilevyille.

Lisätietoja ESD:stä

Videot

Tutustu tuotteen sovellusesimerkkeihin eri toimialoilla - käyttäjäystävällinen, informatiivinen ja käytännöllinen.

Eikö sopivia videoita löytynyt? Tutustu sitten mediakeskukseemme.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

URL-osoite, jota yrität käyttää, ei ole oikeassa kieli- tai maakontekstissa.

Tiliin liittyvä myymälän kanava ei vastaa pyydetyn URL-osoitteen kanavaa. Jos haluat tarkastella hintoja tai tehdä tilauksen, vaihda käyttäjäkohtaiseen kanavaan.

0 tuotteet lisätty onnistuneesti ostoskoriin

Mene ostoskoriin

Schmalz Select - Suositeltava tuotevalikoima alipainetegnologiaan

Kaikki saatavilla. Kaikki valmiina. Kaikki selvää.

Select-valikoiman avulla voit luottaa hyväksi todettuihin vakiotuotteisiin, jotka ovat välittömästi ja maailmanlaajuisesti saatavilla ja joita voidaan yhdistellä optimaalisesti. Ei enää pitkiä toimitusaikoja ja epävarmuutta tuotteiden valinnassa. Löydät juuri tarvitsemasi komponentit - nopeasti, mutkattomasti ja maailmanlaajuisesti saatavilla.