Schmalz

Handling of Cured FRP Components

The cured, often still hot components have to be gripped securely during removal from the tool, without leaving marks on the workpiece. Suction cups made of HT1 are ideal for this process. These suction cups are heat-resistant and free of substances that contain silicone or could impair painting processes. If FRP components are to be coated at a later stage, this avoids possible surface imperfections.

Tuotekysely
Vaatimukset

Requirements for Vacuum Technology

Removal of cured CFRP components

  • The cured components, which are often still hot, must be gripped securely during removal from the RTM mold without leaving any residue

  • Handling during removal of the cut-out parts (preforms) and layers

  • Process-safe handling of the blanks

  • Handling of possibly several layers or unstable preforms

Temperature resistance

  • High temperatures with thermoplastics require temperature-resistant grippers

  • When handling hot workpieces, local cooling at the gripping point must be avoided in particular. Special needle grippers and vacuum cups are used to minimize the risk of excessive cooling. Contact area made of Teflon "non-stick" and thermal insulation additionally prevent local cooling down

Accuracy v. deposit, contamination Gripper

  • Molten components lose their stability and are therefore difficult to handle. Special flat suction pads have a flat, long sealing lip and a support mounted in the suction pad

  • High acceleration possible due to high holding forces

  • High level of handling know-how prevents changes in material properties, e.g. due to damage or contamination

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

URL-osoite, jota yrität käyttää, ei ole oikeassa kieli- tai maakontekstissa.

Tiliin liittyvä myymälän kanava ei vastaa pyydetyn URL-osoitteen kanavaa. Jos haluat tarkastella hintoja tai tehdä tilauksen, vaihda käyttäjäkohtaiseen kanavaan.

0 tuotteet lisätty onnistuneesti ostoskoriin

Mene ostoskoriin

Schmalz Select - Suositeltava tuotevalikoima alipainetegnologiaan

Kaikki saatavilla. Kaikki valmiina. Kaikki selvää.

Select-valikoiman avulla voit luottaa hyväksi todettuihin vakiotuotteisiin, jotka ovat välittömästi ja maailmanlaajuisesti saatavilla ja joita voidaan yhdistellä optimaalisesti. Ei enää pitkiä toimitusaikoja ja epävarmuutta tuotteiden valinnassa. Löydät juuri tarvitsemasi komponentit - nopeasti, mutkattomasti ja maailmanlaajuisesti saatavilla.