Schmalz

Handling of Cured FRP Components

The cured, often still hot components have to be gripped securely during removal from the tool, without leaving marks on the workpiece. Suction cups made of HT1 are ideal for this process. These suction cups are heat-resistant and free of substances that contain silicone or could impair painting processes. If FRP components are to be coated at a later stage, this avoids possible surface imperfections.

Productaanvraag
Vereisten

Requirements for Vacuum Technology

Removal of cured CFRP components

  • The cured components, which are often still hot, must be gripped securely during removal from the RTM mold without leaving any residue

  • Handling during removal of the cut-out parts (preforms) and layers

  • Process-safe handling of the blanks

  • Handling of possibly several layers or unstable preforms

Temperature resistance

  • High temperatures with thermoplastics require temperature-resistant grippers

  • When handling hot workpieces, local cooling at the gripping point must be avoided in particular. Special needle grippers and vacuum cups are used to minimize the risk of excessive cooling. Contact area made of Teflon "non-stick" and thermal insulation additionally prevent local cooling down

Accuracy v. deposit, contamination Gripper

  • Molten components lose their stability and are therefore difficult to handle. Special flat suction pads have a flat, long sealing lip and a support mounted in the suction pad

  • High acceleration possible due to high holding forces

  • High level of handling know-how prevents changes in material properties, e.g. due to damage or contamination

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.