Vacuum Lifting Devices VacuMaster Basic
- For lift capacities up to 750 kg
- Ergonomic operator handle
- Malfunction-free manual sliding valve with clamp-safe catch lever
Loading a CNC punching laser machine used to be done by hand. This task required two to three people. As a general rule, the metal sheets weigh 150-190 kg and measure 2,000-3,000 x 1,000-1,500 mm (length by width). Even when they had enough people, the work was still very hard on the employees and did have an impact on their health.
The vacuum lifting device VacuMaster Basic is the ideal tool for handling sheet metal. Its ergonomic operator handle makes the work easier, without endangering the employees’ health. The operating units of the lifting aid are mounted directly on the handle and make it easy to use. With a maximum load of 190 kg, the lifting device VacuMaster Basic is perfectly suited for transporting metal sheets. The lifting device can be operated by one person alone. The electronic warning device ensures safety: it warns the employee in time in the event of a drop in pressure.
Discover application examples of the product in various industries - user-friendly, informative and practical.
No suitable videos found? Then take a look at our media center.