Schmalz

Bag Lifter

Bag lifters are used in various industries to make it easier to grip, move and then deposit heavy and bulky bags. Schmalz bag lifters are operated with a vacuum. Vacuum lifters are available for various Schmalz lifting aids: JumboFlex, JumboErgo and JumboSprint..

Schmalz lifting aids can support a variety of handling processes.

연락처 찾기

Bag Lifters for Easy Handling of Heavy Bags

Bag lifters make it easier to handle heavy bags in various transport and handling processes. Tube lifters are used for palletizing, lifting and lowering or transporting bags, ensuring greater efficiency as well as ergonomic and fatigue-free working. Schmalz vacuum-operated systems can be adjusted to bags with different contents and weights and enable easy, quick and safe handling of heavy and unwieldy loads.

Bag Lifters for Ergonomic, Fatigue-Free Working

The bag lifters from Schmalz are known as tube lifters, which are divided into three different model types: The tube lifter JumboFlex, for example, enables lighter bags weighing up to 50 kg to be transported at high speeds, while the JumboSprint and JumboErgo models are designed for heavy loads of up to 300 kg. These two models have different operator handles: While the bag lifter is mainly recommended for large-area workpieces and is equipped with a twist grip for easy handling, the JumboSprint has a circumferential bow-shaped handle that allows the bag lifter to be precisely positioned on the bags.

With a large selection of grippers available, the Schmalz tube lifters can be adapted to suit each workpiece and load: For example, there are special bag grippers—including round vacuum grippers with skirts for plastic bags—as well as double and multiple vacuum grippers for all kinds of cardboard boxes. The grippers developed for bags attach securely to the surface of the load and adapt flexibly to its shape. The support grid prevents the vacuum grippers from breaking the bag or sucking it in. The individual grippers can be changed quickly, easily and without tools.

Schmalz bag lifters: Increased productivity, fewer staff absences

Schmalz bag lifters are increasingly replacing the frequently used claw grippers and boast significantly better cycle times, simple handling and a high degree of stability and safety. The systems relieve employees of a large number of work steps and ensure fewer staff absences, higher employee motivation and less tiring work. At the same time, the use of the bag lifters ensures that the handling speed remains at a high level and does not gradually decrease, as is the case with manual handling of heavy loads. Working times can often be made even more efficient and shortened using vacuum lifters.

The Right Bag Lifter for Every Vacuum System

Our experienced Schmalz system consultants will be happy to help and advise you in designing the right vacuum system for your requirements — contact us for information!

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

액세스하려는 URL이 올바른 언어 또는 국가 컨텍스트에 맞지 않습니다.

계정에 연결된 스토어 채널이 요청된 URL의 채널과 일치하지 않습니다. 가격을 확인하거나 주문하려면 사용자별 채널로 전환하세요.

0 장바구니에 제품이 성공적으로 추가되었습니다.

장바구니로 이동