Schmalz

Vacuum Plate Lifter

With vacuum plate lifters from Schmalz, you can effortlessly handle wooden boards, planks and other workpieces. With the help of vacuum, the lifting aids lift the workpieces leaving few marks, but with power. Schmalz offers two types of vacuum plate lifters: The vacuum tube lifter Jumbo and the vacuum lifting device VacuMaster. With the Jumbo tube lifter, you can effortlessly lift loads weighing up to 300 kilograms. The VacuMaster lifting device can lift up to 2,000 kilograms as standard. On request, we can also manufacture devices that can lift and move even heavier workpieces.

Working ergonomically with vacuum plate lifters

The constant moving of heavy loads has a detrimental effect on the psyche and physique of your employees. By using vacuum plate lifters, handling the bulkiest workpieces becomes child's play. In this way, you create an ergonomic working environment and prevent damage to health. The vacuum lifters are supplemented by an aluminum crane specially adapted to your lifting process. This is particularly responsive and also supports ergonomic working methods.

Large product portfolio from Schmalz

Schmalz offers a large product portfolio of ergonomically designed lifting aids. So you can be safe in the knowledge that we will find exactly the right vacuum plate lifter for your application. The Jumbo tube lifter, for example, comes in the variants JumboFlex, JumboErgo and JumboSprint. With the JumboFlex tube lifter, you can handle loads weighing up to 50 kilograms with a practical one-hand operation. For heavier loads, the JumboErgo or the JumboSprint , which is particularly suitable as a bag lifter, are used. The JumboSprint is also available in an Ex version for lifting operations in potentially explosive atmospheres.

Our second vacuum plate lifter, the VacuMaster, is also available in different variations. Depending on the version, planks, coils or even rotor blades for wind turbines can be lifted and moved effortlessly. As standard, we also manufacture vacuum plate lifters that allow the workpiece to be swivelled through 90° or rotated through 90°.

Our experienced system consultants are on hand to help you choose the right vacuum plate lifter.

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.