Matrix-Plates MPL
- Basis of the modular system for metal and plastics processing
- Low-distortion clamping of flat workpieces
- Adaptable to all common machine tables
When separating small electronic components in a CNC machining center, the components have to be clamped using a vacuum such that they do not become damaged or distorted. The matrix-plate in combination with a steel plate and a special film is suitable for this.
The application shows a Matrix-Plate in combination with a Steel-Plate and a special foil in use on a CNC machining center. Aim of the process is the separation respectively, the processing of small electronic parts. With the use of vacuum, these sensitive parts can be hold with no damage and deformation. Damages, which can occur due to vibrations during the process, can be avoided by the areal clamping force. The vacuum is generated by the powerful vacuum unit from Schmalz. The vacuum generator is the ideal product for the application on a CNC machining center due to a broad power spectrum, standard vacuum and level monitoring, acoustic and optical warning device as well as an excellent fluid compatibility.
Discover application examples of the product in various industries - user-friendly, informative and practical.
Nisem našel primernih videoposnetkov? Potem si oglejte naš medijski center.