Schmalz

Claw pump

The claw pump is an electrical vacuum generator that operates with two counter-rotating, claw-shaped rotors. These displace air without contact, enabling completely dry operation without the need for lubricants. This makes electric claw pumps particularly efficient and low-maintenance.

In wood processing, the claw pump is used in the gantry transfer of wooden beams and in automated processes in sawmills and joineries, for example when removing boards. It is also used in the packaging industry, for example when handling cardboards in the carton erector. Thanks to its stable and uniform vacuum, the claw pump is suitable for a wide range of applications in industrial automation.

Related terms

Diaphragm pump
The diaphragm pump is an electrical vacuum generator with a flexible diaphragm. It has a compact design, requires little oil during operation and is low-maintenance.
Electrical vacuum generation
Electrical vacuum generation creates vacuum without the use of compressed air. It is used in industry and logistics to make processes energy-efficient and flexible.
Rotary vane pump
The rotary vane pump is a vacuum generator that uses rotating vanes to reliably generate vacuum and can be used for a wide range of applications.
Side channel blower
Side-channel blowers, also known as side-channel compressors, ensure stable vacuum performance in production and automation with their special flow principle.
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico