Schmalz

Predictive maintenance

Predictive maintenance is a modern maintenance strategy in which the condition of machines and systems is continuously monitored and analyzed with the help of predictive analytics, artificial intelligence (AI) and machine learning. The aim is to reduce downtime, avoid stoppages and extend the service life of machines.

In contrast to reactive maintenance (only repairing when something breaks) and preventive maintenance with fixed intervals, predictive maintenance relies on condition monitoring and real-time data analysis. This allows maintenance measures to be initiated proactively and at exactly the right time.

How does predictive maintenance work?

Predictive maintenance is based on the continuous recording of machine data obtained via IoT sensors. Various parameters such as vibrations, temperature, pressure and audible signals are monitored. The collected data is then analyzed using machine learning algorithms. In this way, the system recognizes patterns and anomalies and creates predictive models that indicate when a component is likely to fail. This allows spare parts to be installed in good time, maintenance to be seamlessly integrated into the production process and unplanned downtime to be avoided.

Products

Challenges during implementation

However, the implementation of predictive maintenance is complex. Companies are faced with the challenge of collecting and processing large amounts of high-quality data (big data), defining suitable limit values for load and wear and building a powerful data infrastructure. In addition, digital models of the machines must be developed, AI algorithms must be trained and the solution must be integrated into existing maintenance processes. Only through the interaction of these factors can predictive maintenance develop its full potential.

Areas of application for predictive maintenance

Predictive maintenance is used in many industries. In production and manufacturing, it optimizes maintenance processes and lowers costs. In mechanical engineering, it is a core component of Industry 4.0 standards. In the automotive industry, it helps to avoid unplanned repairs, while in aviation and rail transport it increases the safety and availability of vehicles and systems. It also plays a central role in the energy industry (e.g. wind turbines).

The future of predictive maintenance in Industry 4.0

With increasing digitalization, IoT networking and the use of AI-supported data analysis, predictive maintenance is becoming the standard in the smart factory. It is considered one of the most important building blocks of Industry 4.0, as it increases productivity, lowers costs and makes companies fit for the future.

Related terms

Digital Twin
Digital twins are virtual images of real objects or processes that use data to precisely replicate their properties and behavior.
Production 4.0
Production 4.0 describes the transformation of production work toward an intelligent factory. Networked products and systems make production more flexible and efficient.
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico