Schmalz

SCPL multi-stage compact ejector: flexible all-rounder

Its high suction capacity and numerous equipment options make the SCPL multi-stage compact ejector from Schmalz universally applicable. It handles different workpieces in a safe process and can be expanded in a modular fashion if required.

Thanks to its high suction capacity, the SCPL multi-stage compact ejector handles porous materials such as cardboard and packaging materials with ease.

Porous or suction tight, large or small: The SCPL multi-stage compact ejector adapts flexibly to a wide range of process parameters. Thanks to its high suction capacity, it moves porous workpieces such as cardboard and packaging materials with ease. An optional air-saving regulation allows it to efficiently handle even suction tight materials such as glass or sheet metal. Schmalz relies on multi-stage nozzles and thus achieves efficient vacuum generation with low compressed air consumption. The result: SCPL impresses in processes with high volume flow requirements while optimizing energy consumption.

Another possible application is large vacuum systems with partial occupancy. Here, the compact ejectors compensate for leakage flows that occur when handling workpieces with different air permeability and keep the vacuum level constant. In combination with surface gripping systems and suction traverses, these all-rounders also evacuate large volumes in unison.

Guard included

Schmalz has integrated the valve technology and vacuum monitoring into the device - operators can therefore dispense with external solutions for controlling the vacuum system. The compact ejector can be controlled centrally via an integrated M12 connector - for quick and easy start of operations. The compact ejector is available either as the basic model SCPLb or in the monitored variant SCPLc. The latter has an electrical connection for controlling the integrated valves and the vacuum switch as well as an LED display. All devices are achieved with a degree of protection of IP54.

Media contact

The Schmalz press team will be happy to answer any questions you may have.

presse@schmalz.de

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

Adresa URL, na kterou se snažíte získat přístup, není ve správném jazykovém kontextu nebo kontextu země.

Kanál obchodu přidružený k vašemu účtu neodpovídá kanálu požadované adresy URL. Chcete-li zobrazit ceny nebo zadat objednávku, přepněte na kanál určený pro vašeho uživatele.

0 produkty úspěšně přidány do košíku

Přejít do nákupního košíku