Schmalz

Operating principles of vacuum generation

Venturi principle

Operating principle

  • Pneumatic vacuum generators function based on the Venturi principle
  • Compressed air is introduced into the ejector (A)
  • Due to the reduced cross-section of the motive nozzle (the Venturi nozzle [B]), the compressed air is accelerated. The dynamic pressure increases, while the static air pressure simultaneously decreases.
  • Once it has passed the motive nozzle, the accelerated air expands and a vacuum is generated
  • Air is "sucked" through the vacuum connection (D) into the ejector
  • The compressed air escapes from the ejector through the silencer (C) together with the "sucked-in" air.

Advantages

  • Vacuum generators that function according to the Venturi principle are especially suitable for very high accelerations
  • Vacuum grippers can be controlled individually
  • Ejectors in different designs for centralized and decentralized vacuum generation depending on the application
  • Various power classes to suit the workpiece and application

Bernoulli's principle

Operating principle

  • Pneumatic operation with integrated vacuum generation
  • Compressed air escapes through holes in the suction cup and is greatly accelerated when doing so
  • Due to the increase in speed, the static pressure falls and a vacuum is produced (A) ("Bernoulli Equation")
  • The accelerated air escapes to the side (B); an "air cushion" is produced between the floating suction pad and workpiece
  • Leakage is compensated for through a high flow rate, which means that even porous workpieces can be handled and separated
  • The Bernoulli effect ensures that the workpieces are handled with minimal contact
  • Floating suction cups function according to Bernoulli's principle

Advantages

  • Low-contact, gentle handling of thin and sensitive workpieces thanks to the Bernoulli effect
  • Safe separation of thin and porous workpieces

The Coanda principle

Operating principle

  • Pneumatic operation with integrated vacuum generation
  • With the Coanda principle, compressed air is guided through an annular gap which accelerates it
  • The increase in the flow speed results in the "Coanda effect" in which the escaping air follows a convex surface
  • The air flowing along the surface produces suction ("entrainment") in the ambient air

Advantages

  • High suction rate and low air consumption (the required operating pressure is 1 to 5 bar) due to the Coanda effect
  • Large contact surface with narrowly positioned vacuum openings prevent the workpiece from being sucked in or damaged
  • Suction areas can also be partly engaged

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

The URL you are trying to access is not in the correct language or country context.

The store channel associated with your account does not match the channel of the requested URL. To view prices or place an order, please switch to your user-specific channel.