Schmalz

Humanoid Robots: The Technology That Is Transforming Entire Industries

Humanoid robots are considered one of the most significant technological developments of our time. Unlike traditional industrial robots, which are typically stationary and designed for a single task, humanoid systems mimic the human form and range of motion. This design allows them to move through environments originally designed for humans - without requiring any modifications to production facilities, storage facilities, or workplaces. This is precisely what makes humanoid robots so promising for the industry of the future.

The Biggest Challenge: Reliable Gripping

While humanoid robots have made tremendous advances in locomotion, balance, and perception in recent years, one capability remains particularly challenging: grasping.

The human hand is a highly complex tool - it can grasp a wide variety of shapes, weights, and materials without causing damage. Humanoid robots therefore require grasping solutions that:

  • are lightweight, so that the robot’s payload capacity and energy efficiency are optimally maintained

  • are compactly designed to operate collision-free even in tight and dynamic environments

  • operate self-sufficiently, without relying on an external compressed air supply or complex cabling

  • grip reliably and precisely, even with varying workpiece geometries and properties

Schmalz addresses this need with the electric vacuum end effector HXCB - a solution for reliable handling with humanoid robots.

Schmalz brings decades of vacuum expertise to humanoid robotics, setting new standards for autonomous gripping with its unique technology.
∼ Markus Schmider, Industry and Key Account Manager Robotics

Vacuum Grippers: The Underrated Robot Hand

In humanoid robotics, there is frequent discussion about increasingly complex gripping systems. However, for many industrial applications, maximum dexterity is not necessary at all. Especially when handling cardboard boxes, containers, and other flat workpieces, the vacuum principle stands out for its simplicity rather than complexity. Vacuum grippers enable fast, safe, and repeatable gripping with minimal mechanical and control-related effort. No complex controls, no sensitive joints - just targeted functionality. This reduces investment and maintenance costs, minimizes potential sources of error, and increases process reliability during continuous operation. For many applications in logistics and production, the vacuum hand is therefore not only the more economical solution but also the more technically efficient one.

Vacuum Grippers for Humanoid Robots: The Benefits at a Glance

NEW: Electric Vacuum End Effector HXCB

The Cutting-Edge Vacuum Gripper for Humanoid Robots

The electric vacuum end effector HXCB is the first to combine an integrated electric vacuum generator with a vacuum gripper in a compact system designed for humanoid robots that need to move freely and handle objects safely. An internal pressure sensor intelligently regulates power consumption - ensuring maximum energy efficiency without relying on external power sources.

image.alt

Applications of Humanoid Robots with Vacuum Grippers

Intra-logistic and Storage

Intra-logistic and Storage

Picking, Sorting, and Transporting Goods

(De-)Palletizing

(De-)Palletizing

Loading and unloading machinery

Loading and unloading machinery

Contact

If you have any questions, we will be happy to assist you.
Schmalz d.o.o.

Velika Ligojna 4
Vrhnika

Slovenija
+386 70 613 796
info@schmalz.si
Contact

Frequently Asked Questions

What sets Schmalz's new vacuum gripper for humanoid robots apart?

The vacuum gripper was developed specifically for humanoid robots and enables safe gripping of smooth and air-tight surfaces. It combines a lightweight, compact design with an integrated electrical vacuum generation system, providing a practical solution for numerous handling tasks in industry and logistics.

What advantages do vacuum grippers offer over complex gripping systems or humanoid robotic hands?

Vacuum grippers are based on a relatively simple and cost-effective operating principle. Unlike complex robotic arms, they do not require sophisticated mechanical systems, sensors, or complex control algorithms. As a result, they are more robust, less prone to malfunctions, and offer the potential for a longer service life while also reducing operating and maintenance costs.

How is it possible to achieve vacuum generation despite the weight and space constraints of humanoid robots?

A compact electrical diaphragm pump generates the required flow rate and vacuum directly within the gripper. This allows sufficient holding force to be designed - despite limited installation space and low weight - to safely grasp and transport objects.

What technical requirements and interfaces are necessary for integration into humanoid robots?

Thanks to a standardized ISO flange configuration - as is also common with cobots - the gripper can be easily connected mechanically. For electrical control, four pins are sufficient; these are controlled via the robot’s digital inputs and outputs.

For which industrial and logistics applications was the vacuum gripper developed?

The vacuum gripper was developed specifically for handling flat workpieces, cardboard packages, crates, and boxes. It is suitable for applications in which objects can be safely gripped by their surface and the use of a complex five-finger gripper is not technical or economically necessary.

How can the vacuum gripper be integrated into existing robot control systems and software environments?

The integration has been deliberately kept simple. Control is handled via a 4-pin interface using digital inputs and outputs. This standard is supported by virtually all robots and control systems, so no complex software modifications are required.

What payloads is the vacuum gripper designed for?

The current gripper is designed for payloads of up to 5 kg. In many cases, however, it is not the gripper itself but the payload capacity of the humanoid robot that represents the actual limitation.

What are the limitations of vacuum gripping, and what challenges arise when handling unknown or flexible objects?

Vacuum gripping works best on smooth surfaces that are largely air-tight. Complex 3D free-form parts can often be handled more safely by mechanical grippers or robotic arms. In addition, the integrated electric vacuum generator can only compensate for a limited amount of leakage. Flexible, highly textured, or air-tight workpieces are therefore only suitable for vacuum gripping to a limited extent. For smooth and air-tight objects, however, the vacuum gripper often offers the simpler, more robust, and more economical solution.

What alternative gripping technologies are suitable for humanoid robots, and how do they differ from vacuum grippers?

In addition to complex five-finger grippers, simple parallel grippers are also used. These grippers are also relatively simple and cost-effective in design and may already be sufficient for many applications. Vacuum grippers really shine when it comes to the fast and reliable handling of flat, air-tight workpieces.
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico

Schmalz Select – Preferred Product Range for Vacuum Technology

All available. All set. All clear.

With the Select portfolio, you can rely on proven standard products that are immediately and globally available and can be optimally combined. No more long delivery times and uncertainty when choosing products. Find exactly the components you need – fast, uncomplicated and available worldwide.