Schmalz

Handling System

The term handling is derived from the human hand and is used to describe manual lifting and moving processes of objects, especially in the field of logistics. Handling means changing the position or location of a workpiece, i.e. grasping something, moving it and placing it back at a specific location. Handling systems from Schmalz contribute to increased ergonomics and better working conditions. The handling solutions from Schmalz consist of the Jumbo and VacuMaster lifting devices and a matching crane system.

Find your contact

Vacuum tube lifter Jumbo

With the help of the Jumbo handling system, workpieces such as cardboard boxes, bags or wooden boards weighing up to 300 kg can be moved effortlessly and efficiently. This vacuum lifter is particularly suitable for lifting processes that require fast and frequent movement of the workpiece. The lifting aids can be equipped with the appropriate gripper for almost any application. In addition, special grippers have been developed for handling boxes, batteries or baggage, for example. Replacing a gripper on the Jumbo handling system is quick and easy.

Products

Vacuum lifting device VacuMaster

With the VacuMaster handling system from Schmalz, even heavy loads of up to several tons can be moved safely and ergonomically by just one person. This lifting device is the perfect tool for handling sheets made of metal, wood, plastics or glass. The VacuMaster can be configured according to the load to be lifted and industry-specific requirements.

The ergonomically designed working posture thanks to Schmalz handling systems minimizes absences due to injuries.

Products

Aluminum Cranes

Thanks to their lightweight construction, Schmalz aluminum cranes are the perfect supplement to the Jumbo and VacuMaster handling systems. Whether jib crane or crane system, the aluminum cranes from Schmalz can be adapted to the requirements of the customer and the local conditions on site by means of the modular system.

Products

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen