Schmalz

Vacuum Technology for the Wood Industry

For Various Surfaces and Rough Conditions

Vacuum Technology for Automation

Vacuum technology from Schmalz is used as a gripper system on portals and robots. The gripping solution can be configured and designed individually with a broad range of separate vacuum components, or purchased as a ready-to-connect gripper system for a specific application.

Schmalz has developed suction cups for handling wood that more than meet the requirements of the industry. Their shape has been optimized to allow sealing on the rough, often porous surfaces of the workpieces. Ready-to-connect area gripping systems and suction spiders can be adapted to any requirement that come up in the woodworking industry. They are based on individual components to allow a custom gripper design.

Vacuum Clamping Technology

Wooden boards are processed in CNC machining centers to manufacture furniture and other products. During this process, the flat boards are clamped in the machine. Using vacuum clamping technology, suction is applied to the bottom of the workpieces to hold them securely in place. This allows the workpiece to be processed on five sides without modifying the machinery.

Schmalz offers a broad range of clamping equipment for all table types and various manufacturers. Schmalz offers machine manufacturers and outfitters complete, cross-manufacturer, individualized clamping systems for vacuum-driven machine tables.

Vacuum Lifters and Crane Systems

Because the rough wooden boards, cut pieces, workpieces, assemblies and furniture bodies can have a wide variety of shapes, weights and properties, Schmalz offers two series of vacuum lifters: vacuum tube lifters Jumbo and vacuum lifting devices VacuMaster. A large selection of different suction cups is available for both series. Specially adapted crane systems and jib cranes supplement the vacuum lifters.

Productaanvraag

Til me op, NEXO.

Een exoskelet dat niet alleen het lichaam, maar ook de geest een boost geeft: door gebruikers te helpen zich vanuit een voorovergebogen houding weer rechtop te komen, zorgt het exoskelet voor voorover buigen NEXO Pro voor merkbare verlichting en meer motivatie gedurende de hele werkdag.

Meer informatie
Vereisten

Requirements for Vacuum Technology

Vacuum Technology for Automation

Preventing Double Layers
When handling porous or permeable workpieces such as MDF or particle board, the workpieces can stick together during destacking. With large-area gripper modules from Schmalz, an integrated separating function ensures that vacuum between the boards is halted by restricting the flow of compressed air. In this way, only one workpiece is picked up and held.

Gentle Handling in Furniture Manufacturing Processes
Handling furniture places particular requirements on vacuum technology to leave few marks and prevent damage to the workpieces. Large-area gripping systems from Schmalz are equipped with suction cups or with a special sealing foam. The soft sealing foam makes it possible to handle workpieces without damaging them or leaving marks, so that they can be coated later on without surface imperfections, even after coming into contact with the gripper. The wide range of products includes suction cups made of specially-developed materials from Schmalz.

Handling Layers of small Workpieces after Processing in Nesting Processes
For layers of workpieces that were processed using nesting, extremely small individual pieces must be picked up and transported with as little additional manual work as possible. The nesting gripper SPZ-NG allows you to destack cut pallet layers in just one handling procedure. Different vacuum circuits make it possible to split the gripper into individual segments. Individual vacuum circuits can be switched on or off as needed, for example in order to avoid picking up certain workpieces during gripping.

Handling Workpieces with Gaps
The large-area gripping system FXP/FMP is used for handling workpieces with large gaps, such as doors with cut-outs for windows. The universal gripper is equipped with a special sealing foam and valve components. This makes it possible to handle doors with narrow frames and large openings.

Working in dusty Environments
When handling lumber, sheet materials, laminated beams, construction timber, CLT sheets, pallets or simply natural materials, knot holes, cracks and damaged material with rough surfaces can make it difficult to use standard solutions. The patented large-area gripping system FMHD was especially designed for these conditions. The large-area gripping system FMHD can also be used effortlessly in environments with large dirt particles, in wet environments, cold environments and when working with resin.

Handling Wood Veneers
The thin wooden layers are extremely delicate and can be cracked easily during transport. Schmalz large-area gripping systems ensure particularly gentle handling of instable workpieces, which allows you to destack and transport veneers without cracking or damaging them.

Vacuum Clamping Technology

  • In woodworking, vacuum technology is used in many process steps for efficient handling and clamping. Automated or manual handling solutions from Schmalz are particularly suitable for loading and unloading machines and for fixing workpieces.

Increasing the flexibility of CNC machining centers

  • Any CNC machining center can be retrofitted with the vacuum clamping system, regardless of manufacturer and type. The modernization enables fast and flexible retooling for frequent product changes - for efficient production processes from batch size one. Schmalz thus offers an economical alternative to investing in a new machine.

Clamping with vacuum in CNC machining

  • CNC machining generates high cutting forces that require secure clamping. Structured surfaces present an additional challenge. Clamping with vacuum blocks ensure secure fixation of workpieces during machining. Suction plates with optional sponge rubber sealing edge improve the fixation of structured workpieces.

Vacuum Lifters and Crane Systems

  • Wood panel handling - Coated particleboard requires gentle handling to prevent surface damage.

  • Panel sizing - Sawdust makes handling difficult when loading and unloading saws and CNC machining centers. Handling with vacuum enables safe transport and thus short cycle times.

Production and further processing of wood-based materials 

  • Uncoated wood-based panel destacking - Separator vacuums prevent unwanted removal of double layers when destacking porous panels.

  • Spring plungers provide gentle touchdown on sensitive materials and minimize tear-off force. 

Handling of prefabricated wood parts

  • Vacuum tube lifters JumboErgo and lifting devices VacuMaster enable fast loading and unloading of joinery systems. Ergonomic material feeding of framing stations and wall production lines are also easy to solve with vacuum handling devices.

  • Swiveling, rotating and turning of the workpieces are possible.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.