Schmalz

From overexertion to permanent incapacity for work

Anyone who lifts, carries, pushes or pulls loads every day puts their body to the test. Often unnoticed and for years - until it's too late. Back pain, joint problems and chronic overuse injuries are among the most common health consequences of physical work. In particular, incorrect strain at work is considered a driver of back problems and other musculoskeletal disorders (MSDs) - currently the most common cause of incapacity to work at almost 25%.
For many employees, manual handling without ergonomic support means: loads that are too heavy, incorrect movement sequences, unfavorable postures - and long-term health risks.

Figures that speak for themselves

162

million days of absence due to musculoskeletal disorders.

21,5

billion euros in annual production downtime costs.

> 20.000

new retirements due to musculoskeletal and connective tissue diseases.

20,8%

of diagnosis days due to musculoskeletal disorders.

Our staff is the key to our great success and we support them. This naturally includes reducing physical strain wherever possible.
∼ Frank Januschowski, Logistics Manager, FreiLacke

Health consequences of unergonomic workplaces

Unergonomic workstations not only lead to short-term discomfort, but can also cause serious long-term damage to health. These consequences affect various parts of the body and have a negative impact on employees' physical well-being, performance and quality of life. Pain, tension and exhaustion are often only the first signs. If the causes are not addressed, they can lead to chronic illnesses and incapacity to work.

Unergonomic working methods put strain on the whole body

Unergonomic working methods not only affect certain areas of the body, but the entire body. Poor posture, repetitive movements and one-sided strain lead to a chain reaction of complaints that can affect different parts of the body. From the neck and shoulders to the back, joints and cardiovascular system - the consequences are manifold and can have a lasting impact on employees' health and performance. The following body regions are particularly stressed during lifting, holding and carrying:

Lower back

Lower back

Elbow

Elbow

Wrists

Wrists

Hip

Hip

Neck and upper back

Neck and upper back

Shoulder and upper arms

Shoulder and upper arms

Knee

Knee

Maintain health, safe power with certified ergonomics

Ergonomic handling solutions are crucial for relieving the body in a targeted manner, preventing complaints and counteracting chronic illnesses. An ergonomically designed working environment is essential, especially in working areas with a high level of physical strain - such as production and logistics.

Aktion Gesunder Rücken (AGR) e.V., in cooperation with Germany's two largest back school associations, has established a quality seal that serves as a guide when selecting workplace equipment. Every product awarded the seal has undergone a detailed certification process. Vacuum lifting devices from Schmalz are certified with the AGR seal. An independent panel of experts confirms: vacuum lifting devices promote ergonomic lifting, enable back-friendly work, accelerate processes, and reduce health-related absences.

More information on the AGR seal of approval

AGR certified Schmalz products

Your health is priceless - lifting technology pays off

Ergonomic lifting technology can significantly reduce strain - and thus avoid downtime and costs.
Use the amortization calculator and see when the purchase pays off.

Start calculation now

Best practice: focus on ergonomics and health

When the focus is on health and well-being, sustainable success is the result: our best practices show how ergonomic vacuum lifting devices noticeably relieve employees, boost their performance and give them more power for demanding tasks - for less fluctuation and a happier team.

Contact

If you have any questions, we will be happy to assist you.
Schmalz d.o.o.

Velika Ligojna 4
Vrhnika

Slovenija
+386 70 613 796
info@schmalz.si
Contact

Frequently Asked Questions

How can I tell if a workplace poses a risk of physical strain?

A risk of physical strain is evident in the task itself—not just when symptoms appear. Two approaches can help with the assessment:

  • Observe the workplace: A workstation is considered high-risk if lifting repeatedly occurs above shoulder height or below knee height, rotational movements occur while carrying a load, loads cannot be gripped, or cycle times do not allow for recovery periods.

  • Systematic evaluation: The risk assessment pursuant to Section 5 of the German Occupational Safety and Health Act (ArbSchG), supplemented by the BAuA’s key characteristic method, makes load weight, frequency, and body posture objectively comparable. In addition, sick leave rates per workstation and feedback discussions provide further insights.

Why can forced postures and repetitive movements lead to permanent damage?

Forced postures and repetitive movements can cause permanent damage if the strain exceeds the ability of muscles, tendons, and joints to recover. Three mechanisms are responsible for this:

  • Reduced blood flow during static strain: Prolonged muscle tension compresses the blood vessels. The resulting lack of oxygen supply can lead to tissue acidification and hardened muscle areas (myogelosis).

  • Microtrauma caused by repetition: Repetitive movements create microscopic tears in the tissue of tendons, muscles, and ligaments. If recovery periods are insufficient, these microtraumas accumulate and lead to chronic inflammation, such as tenosynovitis.

  • Degeneration of cartilage and intervertebral discs: Uneven pressure distribution within a joint exerts particularly strong localized stress. As a result, cartilage and intervertebral discs can lose their cushioning function, accelerating natural wear and tear.

The key factor is the balance between exertion and recovery: Without adequate breaks and ergonomically appropriate relief, reversible symptoms can develop into permanent structural damage.

What are musculoskeletal disorders, and how do they develop in the workplace?

Musculoskeletal disorders (MSDs) are conditions and signs of wear and tear affecting muscles, tendons, ligaments, joints, and the spine. Unlike a work-related injury, they do not result from a single event but develop gradually over months or years. Typical conditions include herniated discs, osteoarthritis, tendonitis, and carpal tunnel syndrome.

In manual work processes, they result from the interaction of three factors:

  • Use of force: Lifting, carrying, pulling, and pushing without mechanical assistance.

  • Posture: Bending, twisting the upper body, or working overhead.

  • Duration and repetition: Repetitive movements without sufficient rest periods.

The combination of these factors is crucial: Only when several factors coincide and exert their effects over a length of time do temporary symptoms develop into permanent damage.
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
Kanal trgovine, povezan z vašim računom, se ne ujema s kanalom zahtevanega URL-ja. Če si želite ogledati cene ali oddati naročilo, preklopite na kanal, ki je značilen za vašega uporabnika.

0 izdelki uspešno dodani v košarico

Pojdi v nakupovalno košarico

Schmalz Select – Preferred Product Range for Vacuum Technology

All available. All set. All clear.

With the Select portfolio, you can rely on proven standard products that are immediately and globally available and can be optimally combined. No more long delivery times and uncertainty when choosing products. Find exactly the components you need – fast, uncomplicated and available worldwide.