Schmalz

Vacuum Technology for the Plastics Industry

Removal of Hot Plastics Leaving Few Marks

Vacuum Technology for Automation

In the plastic processing industry, molded parts, fibers, plastic films or semi-finished products are produced using granulates or powder. Depending on the requirements, the plastics can be adapted to a wide variety of conditions. Their temperature resistance, elasticity and resistance to chemicals make plastics essential to industrial applications. Thanks to their versatility, plastics are now used in virtually all sectors. Whether as packaging materials and insulation, or for use in the automotive industry, plastics are an important component in all industrial applications.

Schmalz offers a wide variety of vacuum solutions for handling plastics: Specially developed high-temperature-resistant materials allow handling leaving few marks even when workpieces are still hot, while extremely compact vacuum generators provide maximum dynamics and process reliability.

Vacuum Lifters and Crane Systems

Schmalz offers vacuum lifters for handling plastics. They relieve operators of the weight of the workpieces and offer ergonomics and efficiency during manual loading of machining tools.

Productaanvraag
Vereisten

Requirements for Vacuum Technology

Vacuum Technology for Automation

Temperature resistance
Plastic parts are often still very hot when they are removed from machines, meaning that conventional suction cups cannot be used. Schmalz suction cups made of the specially developed HT1 high-temperature-resistant material are heat-resistant up to 170°C, making them ideal for handling in the plastics industry.

Ensuring that workpieces can be coated
Suction cups often leave invisible marks on surfaces during handling, which then prevent coatings from sticking later. Schmalz uses special suction cup materials to allow workpieces to be coated completely, even after handling.

Few marks
Thin-walled workpieces require particularly gentle handling without lasting deformation. The flat suction cups SGPN from Schmalz have a very low volume and a supporting surface on the bottom to prevent marks and distortion in the workpieces.

Dynamic processes
Vacuum generators are often too large to mount directly at the operation site. The necessary hoses usually result in increased compressed air consumption. In order to avoid these losses, Schmalz inline ejectors can be integrated directly into the hose line and used even in confined spaces.

Vacuum Lifters and Crane Systems

Ergonomic machine loading and efficient intralogistics with manual vacuum handling devices

  • Handling workpieces made of plastics with vacuum lifting devices. They relieve the operator of the weight of the workpiece and ensure ergonomics and efficiency in the manual loading of processing machines

  • Swiveling handling of plastic workpieces is also possible with manual vacuum lifting devices

  • Heavy weights and large workpiece dimensions can be moved safely with our vacuum solutions

High level of expertise in handling plastic workpieces

  • Gentle handling of sensitive (e.g. painted) plastic surfaces thanks to a wide range of suitable suction pads

  • High level of expertise in handling special plastic workpieces such as starter battery handling or small load carriers

  • Effortless handling of plastic bags by means of special handling solutions and matching suction pads with elastic sealing lip

De juiste tilhulp vinden

Onze configurator toont u de juiste, ergonomisch ontworpen tilhulp - met slechts een paar details over de applicatie en zonder dat u enige productkennis nodig hebt.

Meer over de configurator

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.