Schmalz

Vacuum Technology for the Packaging Industry

Handling Products with Different Properties

The packaging industry is one of the largest growth markets in the world. Packed items such as food, beverages and other consumer goods require a wide variety of packaging. Goods must be protected from spoilage, damage and contamination, while being presented in an attractive and appropriate manner. The food and beverage and pharmaceutical sectors have the most influence on packaging, and their choices are ultimately based on the consumer.

At the same time, the packaged items themselves have many different requirements for packaging materials. Solid, liquid or powdery goods require individual packaging materials such as bottles, tubes, buckets, cardboard boxes and blister packs. This means a wide variety of materials, machines and technologies are required for the packaging industry.

The processes in the packaging industry are essentially divided into primary packaging, secondary packaging and end-of-line palletizing. Vacuum technology from Schmalz is used in all areas of the packaging industry: in suction cups for putting chocolates into trays (primary packaging), in compact end effectors for placing filled bags in a cardboard box (secondary packaging) and in vacuum systems for automated palletizing (EOLP).

Productaanvraag

Webinar: Mobiele robots het vermogen geven om voorwerpen vast te pakken

Ontdek hoe de Smart Vacuümpomp GSP de elektrische vacuümopwekking op een geheel nieuwe manier benadert en nieuwe normen stelt op het gebied van energieefficiency en prestaties – schrijf je nu in!

📆 19 november 2026, om 10.00 uur EST | 15.00 uur GMT | 16.00 uur CET
🎤 30 minuten, inclusief een vraag-en-antwoordronde
🌐 Engels

Over het webinar

Process Steps and Vacuum Solutions in the Packaging Industry

Click on the individual areas to learn more.

1
Vacuum Technology for Processes in the Primary Packaging Sector
2
Vacuum Technology for Processes in the Secondary Packaging Sector
3
Vacuum Technology for Processes in the End of Line Palletizing Sector
Vacuum Technology for Processes in the Primary Packaging Sector

Requirements for Vacuum Technology

Suction cup materials suitable for use with food and beverages
The food and beverage and pharmaceutical industries have the highest standards for suction cup materials. Schmalz offers suction cups made of FDA-compliant materials. These materials can be cleaned with the standard cleaning agents typically used the food and beverage and pharmaceutical industries.

Product recommendations for the primary packaging sector

Vacuum Technology for Processes in the Secondary Packaging Sector

Requirements for Vacuum Technology

Handling both rigid and flexibly packed products
The grippers have to flexibly adapt to different packaging materials. Plastic films can only be gripped by suction cups with particularly flexible sealing lips. Porous, abrasive cardboard boxes require suction cups with excellent sealing properties and particularly long service lives.

Handling blister packs, ampouls, vials and syringes in the pharmaceutical industry
Blister packs, ampules and vials require suction cups with small diameters. At the same time, the products must be safely moved or held in place. The broad range of suction cups also meets the high hygienic requirements.

Product recommendations for the secondary packaging sector

Vacuum Technology for Processes in the End of Line Palletizing Sector

Requirements for the End-of-Line-Process

Palletizing and depalletizing
Entire product layers can be moved automatically with a layer gripping system SPZ or the area gripping systems FXP and FMP. The gripping system doesn’t have to be completely covered with products. The gripping system can be adapted to the individual requirements of the process. In addition, the area gripping systems are so flexible that they can move different products without requiring a gripper change.

Product recommendations for the End of Line Palletizing Sector

Documenten

Video's

Ontdek toepassingsvoorbeelden van het product in verschillende industrieën - gebruiksvriendelijk, informatief en praktisch.

Geen geschikte video's gevonden? Neem dan een kijkje in ons mediacentrum.

Schmalz Companies

Select your Schmalz Company in one of the following regions:

Regions

Your region is not listed?

Schmalz maintains an international sales network with sales partners in over 80 countries. Please select a language for our international website.

De URL die u probeert te openen is niet in de juiste taal of landcontext.

Het winkelkanaal dat is gekoppeld aan uw account komt niet overeen met het kanaal van de gevraagde URL. Om prijzen te bekijken of een bestelling te plaatsen, schakelt u over naar uw gebruikersspecifieke kanaal.

0 producten succesvol toegevoegd aan winkelwagen

Naar winkelwagen

Schmalz Select - Preferent productaanbod voor vacuümtechniek

Alles leverbaar. Allemaal klaar. Alles veilig.

Met het Select-assortiment kunt u vertrouwen op bewezen standaardproducten die onmiddellijk en wereldwijd leverbaar zijn en optimaal gecombineerd kunnen worden. Geen lange levertijden en onzekerheid meer bij het kiezen van producten. Vind precies de componenten die u nodig hebt - snel, ongecompliceerd en wereldwijd leverbaar.